Hi,
It's indiccated in the MSP430x2xxx family user guide "slau144d.pdf" inside figure2-8 that the value of the current consumption in LPM3 is 0.7uA (at Vcc=3V). But if the comparator A+ were active(Comaprator Interrupt is enabled by the bit CAIE of CACTL1 registe), does the value of the current consumption 0.7uA? Or in this case, the current consumption is equal to 0.7uA plus the current consumption of the comparator?
Regards