This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCE/CCS improvements



Hello!

I don't know if I am the only one having these problems (or thinking these are problems),
but here are a few ideas to improve CCS. I have been already writing about it in the past,
sorry about it, but I really think this could greatly improve the IDE.

1. Adding a linked source code folder:

Right-click the project, then choose new->folder. In the popup, choose "advanced" and then
choose the source folder from the file system.
At this point:

  • It would be nice if it could remember the last folder I added, instead of restarting at the
    root of the file system.
  • It would be nice if it could accept links (possibly reconverting them to absolute paths), which
    would be an alternative: in this case, I could put a link on the desktop, which points to my
    source code folder, and then browse to the folder I want to add in less steps.
  • It would be nice if it could remember that I always choose "advanced". Or at least it would
    be nice if it could remember what I chose last time.
  • Usually after adding a linked source folder, its path also has to be added (right click project -> properties
    Then C/C++ build -> include options. Why isn't this path added automatically?
    Is there any trick to make this work without setting the path?
Now if the user must be left the possibility not to add the path, couldn't this be a user preference
in the build settings?

2. Compiling, loading, running

Apparently the load time improved in CCS vs CCE.
However, there is still something I have been wondering about: what is the purpose of launching the
program if the compilation / link failed? Is there any advantage of doing this? (just curious).
This was already the case in CCE3, so probably there is a sound technical reason to allow
to launch a failed program. Could anybody explain?
Now a related issue: in the preferences panel (that was also the case in CCE3), in Run/Debug->Launching,
there are launching options, all with 3 possible settings except one. Why does "Continue launch if project
contains errors" have only 2 possible settings (i.e no "never" option)?

3. Opening a project:

There is apparently only one way to open a project: start CCS, and choose "switch workspace"
to go to the relevant location. At this point, apparently the whole IDE is shut down and restarted
I think it could be nice if a workspace could be opened by double-clicking the workspace
icon. And similarly it would be nice to open a specific project in the workspace the same
way: double click the project file opens the relevant workspace and sets the selected
project as active.

Pascal

**Attention** This is a public forum