I followed the procedures in user guide but no success.
MSP-EXP430F5438 Programming Tool always tell me:
error detected, aborting:
Could not initialize device interface
MSP-EXP430F5438 Programming Tool
Press CTRL+C to terminate job.
Please tell me how to fix it! Many thanks!
-----------------------
1. Populate the three headers on JP4 (SCL, SDA, RST) and insert the MSP430F5438 device into the
socket with pin 1 at the top-left corner of the socket (see Figure 1-1). The jumpers on JP5 may be
used to complete this procedure.
2. Select USB on the Power Switch at the top left of the board.
3. Plug in the mini-USB cable to the mini-USB port on the MSP-EXP430F5438 board.
4. Plug in the other end of the cable to an USB port on the host PC.
5. Run the program.bat batch file in the folder Update_EEPROM and press the key when prompted. The
program has executed correctly when the words "Please install new driver..." appear on the LCD. This
procedure serializes the experimenter board using a unique ID from the TUSB3410. Note that this
procedure can take a long time, up to a full minute.