Other Parts Discussed in Thread: MSP430F2274
Hi,
I have seen some warnings that a simple RC circuit on the /RST pin is not usually enough for a reliable design. I have 47k from Vcc to /RST and then 100nF to GND. I also have a reset switch in parallel with the cap to allow a forced manual reset.
This has proven satisfactory in the past, but I wonder should I use something more sophisticated, e.g. dedicated reset controller IC. Under what circumstances is the RC likely to prove unreliable. I am using the MSP430F2274. The unit's power comes from a LDO regulator (whose input voltage comes from a 24V ->4V DC/DC converter , pretty close by (i.e. within 75mm or so). The unit runs continuously over months.
Tks
Tony