Hi all,
Has anybody tried to use simpliciTI to realize PDF or Word file transfer? I have two eZ430-RF2500 boards with CC2500 on board. Each eZ430 board is connected to a PC respectively via the com port (by using a MAX232 circuit) . I have set up a peer to peer application network. What I am tring to do is to transfer a PDF or a Word file from one side to another using simpliciTI. However, when I try to do this on hyperterminal “send file” option (not "send text file" option). By using Xmodem protocol, I can only manage to transfer 128bytes for PDF and 256 bytes for Word. Anyone can give me some suggestions on how to improve? Is it possible to get large size file transfered? Or anyone can suggest another software to transfer files? I tried tera term and got similar situation. Any help is much appreciated!!!
Regards
snowy beauty