I need to find something will be able to keep 4 12 volt 15-20 ohm solenoids on.
I tried a quad H-driver chip (TI SN754410) that handles 1A and it seemed to overheat.
Thanks for any ideas!
This will be active LOW by the way. I have 4 solenoids with a common 12V and need to give a low signal to the other end of each of the four of them.
EDIT: the driver chip does work. I had LEDs connected in parallel to the solenoids and with a 1.5k resistor in series with the common anode of the leds and 12V supply and they weren't lighting up when I added the load of the solenoids. Need to lower my resistor value. The driver is working. But it is very hot in operation I should add.