This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCO vs Crystal Power comparison

In terms of power efficiency,  how does it compare to use the internal dco vs using a crystal oscillator for sourcing MCLK?

  • Wilberto Lopez said:
    In terms of power efficiency,  how does it compare to use the internal dco vs using a crystal oscillator for sourcing MCLK?

    Driving a crystal generally requires much more power than letting the DCO oscillate. It does, however, provide a way more precise frequency and much lesser temperature drift.

    Example: on 1MHz, the crystal takes ~180µA(calculated down), the DCO ~80µA (LPM2-LPM0 current)

    Also, it is a good idea to keep the crystal on all the time (even in LPM) because it requires some time to settle. The DCO can be switched off and on with only a few µs settling time.

    But if you need precision, then there is no DCO vs. XT question. DCO is disqualified form the beginning :)
    (well using FLL and REFO, precision of the DCO can be significantly increased, bu tis still no match to a crystal and also introduces some jitter to the generated clock frequency)

**Attention** This is a public forum