Hi,
I am going to be writing a Flash monitor/BSL and would like some comments please.
My requirements are that the client can update the code via the existing communication interface using an application I develop that can tap into the comms interface. Portions of the link will be via RF and some via RS485 so the monitor/BSL will be fairly large to accommodate both.
I have read slaa341, slaa149, slaa089, slaa096 and others.
My questions are as follows:
1. Since I can't directly use the TI BSL serial interface do I still use the TI BSL to do the Flashing (well tested), if so is there an interface spec?
2. Do I use a downloadable monitor, advantage is that if it changes then the latest version is always used.
3. Use a permanent monitor/BSL but should it use direct or indirect interrupts?
Thanks,
Charles