Hi,
We are using MSP430F6636's DAC to generate sine wave,
and there is some problem with the DAC output.
When the supply voltage(Vcc) is around 2.8V
the sine wave's min(bottom) level is almost near to the "0"
but when Vcc increases to 3.5V, the sine wave's bottom level
also increases to 1V (instead of staying near "0").
According to the datasheet's "DAC, Output Specifications"
the Output voltage range for the bottom level will be 0.1V at MAX.
Could you please let us know how to keep the bottom level near to "0"
even if there is any voltage(Vcc) fluctuaion.
Regards.
Paddu