This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Make / Link Problems with ez430rf Demo Projects After Trying CCS v4

Other Parts Discussed in Thread: SIMPLICITI

I was having some problems with results on some of the ex430rf demo projects (Accees Point as Data Hub) - and realizing those were originially targetted to IAR, and not CCE, I figured I'd give the beta of CCS v4 a shot and see how that did.

Unfortunately, I cant succeed in building the project anymore.  I keep getting errors such as:

C:\Program Files\Texas Instruments\ccsv4\utils\gmake\gmake: *** No rule to make target `C:/Program Files/Texas Instruments/SimpliciTI-CCE-1.1.0/Components/Components/bsp/bsp.c', needed by `Components/bsp/bsp.obj'.        Project    Unknown    1245905177203    15

I had reinstalled v4 and Simpliciti, in previous versions of the errors is was still aiming at the CCE bin tool versions.  So above it shows updated ccsv4 locations, but still cant build.  I also read through the migrating to v4 document and saw a comment about setting the object file directories in the build options - but that didnt work for me. 

 

Not sure if this matters - but when I originally opened the projects in v4 I used the "existing CCE" project import option - with copy to workspace.  It always complains afterwards about the C/C++ indexer having issues - and I wasnt sure if that was related or not.

Thanks for the help...

 

 

 

 

  • I started again and reimported the project and now I seem to be getting this:

     

    warning: cannot resolve archive C:/Program Files/Texas
       Instruments/ccsv4/tools/compiler/msp430/lib/libc.a to a compatible library,
       as no input files have been encountered
    fatal error: no input files

     

     

**Attention** This is a public forum