I'm investigating a board using a MSP430F148 with a 7.4MHz xtal on XT1. This has proved to be unreliable. VCC is 3.45 so the frequency is only just inside the limit I know. The xtal is <25 and I've done the add some R test to check the safety factor, which is barely 2. I then measured the amp in the MSP430 (on 2 boards). For 500kHz, 0.1Vpp via 100n in, open circuit output, Vout is 1.0/1.5V, at 1MHz this drops to 0.5/0.6V so gain is starting to fall off and at 7MHz I'll be lucky if it >1. And it gets worse. I loaded the 500kHz with 10K + 47n (in series) and the output dropped to 0.5/0.25 giving an output impedance of ~11k/56k. With those figures the mystery is not why it is unreliable but how it ever oscillates in the first place.
I've run the unit with a debugger and kickstart so I know XTS is set. With XTS =0 there is no output at all. TI support say they have no data for this amp so I've no idea if this is just 2 bad units or what. Anyone else measured the oscillator? The knowledge base says xtal <40R is required (mine is <25R). Given that a typical off the shelf xtal is 120R spec then I suspect the oscillator is weak but this weak?