Other Parts Discussed in Thread: MSP430G2452, MSP430G2553
Hi,
We need some advise for our customer's project using G series(MSP430G2452).
This project needs PWM output(100Khz) and a general purpose timer to
produce timely intervals(1ms to 10ms) & to measure the time of PWM output.
(Even the WDT is used for other purpose)
But unfortunately, MSP430G2452 has only one timer(TA3),
we wonder if we could use TA3's three channels to produce 100Khz PWM
as well use it as a general purpose timer.
I have seen some posts & application report about making multiple PWM's out
of one Timer but not with the above scenario.
Please let us know if there is any suggestions to
implement this without going for another device with 2 Timers.
Regards.
Paddu