Q1:
Setting a pin bit in p1sel to 1 that is listed as capable of TA0.1 will toggle/set or reset when TACCR1 is trigged ? (timer-A is enabled)
It can not toggle/set in any form on TACCR0 or TACCR2 triggers?
Q1: If two pins have been TA0.1 enabled, and they are started as one low and one as high,
and using toggle mode only will the outputs be complement of each other?