This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

malloc and free functions halt execution



Hi

My application is rather big, approximately 200 kB. I have set my heap to 6000 kB and my stack to 2000 kB. My compiler is CCE Professional 3.2xxxx. I use the large memory model and large data model and is linking with rts430xl.lib.

I have been getting trouble when using malloc and free. Sometimes they work quite fine and other times they just halt execution, the application stops running and I cannot single-step any further. In one case (application 1) malloc fails, in another (application 2, similar to application 1) free fails. I have been reading about another library called rts430xl_eh.lib, when is it applicable to use that?

Have you experienced anyting similar or know what might be wrong? Any help is of course welcome, hints, tricks and ideas.

/Adde

  • Both the heap and the stack should be in RAM. How much RAM do you have?

  • Thanks for your response.

    Sorry, I meant 6000 and 2000 bytes. Yes, they should be in RAM.

    From my map-file:

              origin           length         used          unused    attr.

    RAM 00001c00 00004000 0000281a 000017e6 RWIX

     

    The stack is located directly beneith FLASH1 in memory:

    .stack 0 00005430 000007d0 UNINITIALIZED

    00005430 00000004 rts430xl.lib : boot.obj (.stack)

    00005434 000007cc --HOLE--

     

    Heap:

    .sysmem 0 00001c00 00001770 UNINITIALIZED

    00001c00 00000008 rts430xl.lib : memory.obj (.sysmem)

    00001c08 00001768 --HOLE--

     

    This seems to be ok I guess. The memory sizes are 6000 and 2000 (0x1770 and 0x07d0) and the positions are right?

    What about this other runtime library I asked about, the one with extension _eh, when is that supposed to be used? I made the memory allocation static for now but this is definitely not a solution.

    Thanks

    /Adde

  • Adde said:
    I made the memory allocation static for now but this is definitely not a solution.

    Just after writing this I single-stepped further in my application and got to the next point malloc are used (small allocation this time),  and execution halted again. Something unexpexted is happening, I have tried increasing the heap size without any results. I have also (until now) assumed malloc returns a NULL-pointer if the allocation fails, not just halt execution.

    I did not answer how much RAM I had earlier. This is 16 kB for my device (the F5438).

    /Adde

     

     

     

     

  • I had a similar problem.

    As source code for malloc() is not available, I single stepped into its assembly, and after about 15 steps, I found myself in the middle of one of my functions, out of the blue...

    It turned out that malloc() is using some pointer to one of its functions, and calling it indirectly (jumping to the address written in this pointer variable).

    Adding a "watch-point" (data break-point) for write access on this variable's address, I found that my code is overwriting it (out of bounds array index), causing malloc() to jump to (call) a function at a wrong address.

  • Generally, stack starts at upper limit of RAM and grows downward. Static and global variables are usually placed at lower limit of RAM and go upwards. The space in the middle is the heap.

    Note that the limits you specify in the linker file are just guidelines. There is nothing that prevents the stack from growing past the bounds you set in linker file and overwriting memory you expect to use as your dynamic allocation heap.

    I would recommend using the debugger to halt your program at the reset vector, then fill RAM with a known pattern (like 0xDEAD) and then run your program until you get your failure condition. Then check your stack range to see if the stack overflowed. Also check that there is still enough 0xDEAD space left to satisfy your malloc() request etc....

    That you should help you narrow down the source issue.

    I use dynamic memory allocation on the 5438A as well, and have no problems. I have a custom memory manager and malloc() implementation however.

  • Hey, Brian, the stuff about the growing stack is my text. :)

    Nevertheless, an index-out-of-bounds write to an array (as it was apparently the case) can write everywhere. Especially since the index is signed, so a negative value will write to somewhere below the intended array destination (not writing in the “DEAD” area). Apparently (in this case) to the space where malloc stores its pointers.

**Attention** This is a public forum