This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am new to CCS and MSP430. I copied CC1100 example code to MSP430F5529 User Experience source code. The project compiles cleanly, but the linker complains about "program will not fit into available memory. placement with alignment fails for section ".int42" size 0x4.
Available memory ranges:
INT42 size:0x2 unused: 0x2 max hole: 0x2
I checked the map file and it shows:
.int42 0 00000000 00000004 FAILED TO ALLOCATE
.int47 0 00000000 00000004 FAILED TO ALLOCATE
How do I easily find two ISRs assigned to same interrupt vector?
Regards,
Ed
Make a text search for the pragma that assigns the vector to the following function.Ed Lombardo said:How do I easily find two ISRs assigned to same interrupt vector?
Either your code indeed has two interrupt functions for the same vector, or your interrupt function is placed above 64k, resulting in a 20/32 bit address which of course won't fit into a 16 bit vector location.
Hi,
I found two #pragma vector instances from MSP430 User Experience project and C1100 project.
Thanks
**Attention** This is a public forum