New Question:
0FFF4 - Watchdog-timer interrupt vector
0FFF4 MOV.B @R6, 0FFFF(R7) Where R6's address is 5644 and contains 33 in that address.
R7's address is 5732
If I understand this correctly the instruction will take the contents of address 5644 and store it in the address 0FFFF +R7
Expanding this out: 0FFFF + 5732 which makes the new address 5731? Is that correct?
Will 33 be stored in address 5731?