I just received an eZ430-RF2500 Eval kit and I cannot seem to connect to the USB dongle. When I follow the instructions in the "eZ430-RF2500 User's Guide" for downloading the demo firmware to the target, IAR Kickstart tells me:
Fatal error: Failed to initialize.
Check if hardware connected.
Check if drivers are installed.
Try to restart the computer.
Tools using the parallel port are not supported on Windows Vista
Session aborted!
Similarly, when I write a simple program in CCE and try and debug it, CCE gives me this error message:
Error initializing emulator:
Could not initialize device interface
I belive that I have the drivers for the dongle installed properly as my Hardware Manager shows all the same devices (correctly) installed as described in the "MSP-FET430 Flash Emulation Tool" document. I've also tried uninstalling and reinstalling the drivers and IAR Kickstart/CCE.
Does anyone have any suggestions to why I can see the dongle in my hardware manager, but still cannot connect?
Thanks,
Brent