Other Parts Discussed in Thread: MSP430FG4617, MSP430FG4618
Hi everyone,
Currently I am working with the MSP430fg4617 in a medical implantable device and I have some questions regarding to use the MSP430 in this kind of application.
1.- I have observed some Medical Implantable Designs using MSP430 microcontrollers on the IEEE Journal database but I am not sure if it is suitable to use them. Does anybody has a recommendation or experience working with any MSP430 in medical implantable devices?
2.- What is the value of R in the schematic that appear in figure 22.5 in the MSP430x4xx User's Guide (SLAU056G)?
3. Using the internal OA's, I may need a gain higher than 15 (the maximum programmable gain) and I am trying to use this stage as antialiasing filter as well. I think that I can I get more gain using external resistors and capacitors but, is it suitable? Are those OA's designed to have that kind of performance?
4. I need as less external components as possible so depending on the value of the R (from question 2) I will try to design an antialiasing filter combining this R with an external cap, is it suitable?
5. From figure 22.1 of the same document mentioned in 2,P430x4xx User's Guide (SLAU056G), it seems that one can use the three op amps independently with different configurations and different gains. If I use OA0 and OA1 in non inverting configuration and OA2 as differential amplifier it looks like an instrumentation amplifier. Is it possible to design an 3 op amp Instrumentation amplifier using the internal OA's of the microcontroller?
6. Does anybody knows about some kind of SPICE macromodel for the internal OA of the microcontroller? I would like to use PSPICE to do some simulations and see if I can reach my specs using them.
Please don't doubt to give me your opinon. Any comment will be very welcome.