This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

potential part substitute

Other Parts Discussed in Thread: MSP430P325, MSP430F425A

we are running into problems with an performance upgrade  using the OTP part MSP430P325.  Is there a ROM/Flash based part which we could seemlessly port the code too, and one that is pin for pin compatable with 325 series?  We have TI flash programmers here, in this way we could flash a part, then test, then re-flash and test, this would be slow.  We can debug also but need to cut into the board to interface to the TI debugger.  any suggestions here?

 

 

**Attention** This is a public forum