I am using the MSP430F2272 and using a USB/UART adapter to connect a PC to the MSP430F2272.
I notice that with the USB/UART adapter plugged in to a USB port on the PC, as soon as I connect the UART side of the USB/UART adapter to the UART pins(TxD, RxD, Gnd) of the MSP430, the MSP430 starts running code. I find that this leakage of power sometimes results in an improper reset of the MSP when power is applied to the MSP.
Has anyone experienced this? Is there a simple way of avoiding this power leakage into the MSP430?
Regards,
Robert