Hi,
Im very new to working with the AIC3254, but would like to configure the codec for playback via I2S.
Im using the low power stereo playback as a rough guide but have so far been unsuccessful at getting audio playback to work.
I have MCLK = 16Mhz and set WCLK and BCLK as outputs, NDAC=1 and MDAC=4, DOSR=64. I
I wish to route audio from the I2S or DIN input to the HP Out and/or LineOut .. without any real processing from the dsp or processing blocks?
Could someone please point me in the right direction? Or give me more information on how I would do this?
Thanks,
Josh