This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Timer B Question

Other Parts Discussed in Thread: MSP430FG4618

I'm just testing out TImer B on the MSP430FG4618.

I've written a simple program to calculate the length of time it takes to initialise an integer array to zero.

The timer is setup using SMCLK which I believe has a frequency of 1 MHz.

After running through the function, the number of clocks on the TBR register is 1170.

From what I gather this corresponds to (1/1MHz)*1170 seconds = 1.17 ms

Does this length of time seem plausible for simply intialising a seventy element array to zero?

 

Here is the code used:-


#include  <msp430xG46x.h>


int i=0,n=0;

int x[70];


void main(void)
{
  volatile unsigned int i;

  WDTCTL = WDTPW+WDTHOLD;                   // Stop WDT
  FLL_CTL0 |= XCAP14PF;                     // Configure load caps

  // Wait for xtal to stabilize
  do
  {
  IFG1 &= ~OFIFG;                           // Clear OSCFault flag
  for (i = 0x47FF; i > 0; i--);             // Time for flag to set
  }
  while ((IFG1 & OFIFG));                   // OSCFault flag still set?


while(1){



TBCTL = TBCLR ; //Clear Timer B
TBCTL = TBSSEL_2+MC_2;                 // Start Timer

for(i=0; i<70; i++){
    x[ i ] = 0;
}

n=TBR ;  // Read Timer Now



}

}

**Attention** This is a public forum