Hello,
I am trying to use EEM trace capability for statistical profiling with TI JTAG adapter. So far no luck. Of all trace modes only "history" seems to work but it "works" only once per session. Emulator and MSP430.dll were updated to v3 and I do have dll code and managed to build it. My MCU does have that enhanced EEM with trace and whatnot.
TI appnotes state that trace works in IAR and CCS so I went to the trouble of installing both to verify it. IAR workbench says that only C-SPY supports trace and this functionality was disabled. CCS also had it greyed out. IAR is v5.40.7, CCS is 5.2. I wonder if trace got broken in dll v3 and latest IAR and TI toolchains?
If anybody managed to get trace working I would appreciate if you could post the sequence of calls to the MSP430.dll and correct arguments.
Regards,
Sergei