With the MSP430G2111, is it possible to program a cap value for PWM or is the max set at VIN and you have to use an analog to digital converter, send the output to an op amp, then through a digital to analog converter? I am trying to program an MSP430G2111 to control several diffrent ic's and some require a specific voltage level (varying from 2.7 V to 9 V)
Thank you in advance!