This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCE V3 : How to format the memory view?

Hello!

I have the following problem with the memory view:

When I want to format the rendering, I can choose the row size (in bytes) and

the column size (also in bytes). The default seems to be 16 bytes grouped by 2

(2 units per columns).

Now I have to deal with text, so I would prefer a rendering in bytes. Therefore

I have configured as 16 bytes per row, and 1 byte per column. It works.

However, these settings don't survive a rebuild. Of course, I have tried to

press "save as defaults", but it doesn't help.

Is there a way to make the changes persistent?

Now  about the memory renderings, I would really like to have one ASCII

rendering together with the hexa (without switching renderings) like in any

good old hex editor. Is this possible?

Thanks,

Pascal

 

**Attention** This is a public forum