This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC question



This function is not executing on CCE compiler, what's the problem?

static void halMcuInit(void)
{
  volatile uint16 tmp = 0;
  int i;
  WDTCTL = WDTPW | WDTHOLD;          // Disable the watchdog.

  // Setup code taken from TI example code: msp430x22x4_adc11_temp.c.
  ADC10CTL1 = INCH_11 + ADC10DIV_3;  // Internal bus voltage, ADC10CLK/4
  ADC10CTL0 = SREF_1 + ADC10SHT_2 + REFON + ADC10ON + ADC10IE;
  /* Allow Vdd to settle before reading it and re-configuring the system clock.
   * MSP FAE confirmed that it can take up to 1 second for the Vdd to settle.
   */
  while (--i);
  while (--i);

  ADC10CTL0 |= ENC + ADC10SC;        // Sampling and conversion start.
  LPM1;
 
 //__low_power_mode_1();              // Low power during sampling period.
  // Clear the signal that the ADC sample is ready - it is only to be used here.

  halAdcval = ADC10MEM;

  halEventFlags &= ~HAL_EVT_ADC;
 
     //ADC10CTL0 &= ~HAL_EVT_ADC;

  // Measurement of AVcc/2 is in range 0 to 1023 indicating voltage from 0 to 1.5V.

  tmp = (halAdcVal * 30 + 512) / 1024;  // Convert to units of 0.1V

  // Cannont use 8-MHz if the Calibration values have been erased or if the bus voltage < 2.2V.

  if ((tmp >= 2.2) && (CALBC1_8MHZ != 0xFF) && (CALDCO_8MHZ != 0xFF))
  {
    // Configure the system clock for 8-MHz by loading the calibrated values from the info memory.
    BCSCTL1 = CALBC1_8MHZ;
    DCOCTL = CALDCO_8MHZ;
  }
  else
  {
    halEventFlags |= HAL_EVT_NO_8MHz;
  }
}
      

Problem is at halAdcVal=ADC10MEM instruction.

**Attention** This is a public forum