This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IAR Compiler, switch() statement, and jump tables


I am writing an interrupt-driven app for the ez430-F2012T target
board, and using three switch/case statement inside two interrupt
handlers.

I'm using the TI-supplied IAR Embedded Workbench compiler,
specifically:

  IAR C/C++ Compiler for MSP430 V4.10E/W32 [Kickstart] (4.10.5.3).

In one case, the IAR compiler generates a very nice jump table.

In a second, it rejects this statement:

  switch (__even_in_range(TAIV,10))

generating the following error:

  Error[Ta021]: This intrinsic can only be used as argument
  to a switch statement

but accepts this:

  switch (TAIV) {

(On an earlier incarnation of this same code, the IAR compiler might
 -- or might not -- generate error TA021 depending on the C
 statements in one of the 'case' sections.)

In a third case, a swtch() inside the TAIV switch(), the IAR
compiler generates a series of SUB.B/JEQ instructions.

Here's a sample of an error-generating switch() statement:

#include "msp430x20x2.h"
int main( void )
{
  switch (__even_in_range(TAIV,10)) {
  case 0:
    break;
  case 2:
    TACCR1 = 0;
    break;
  case 4:
  case 6:
  case 8:
    break;
  case 10:
    break;
  }
  return 0;
}

When I attempt to compile this on my system, it generates an
Error Ta021. If I comment out the TACCR1 line, it compiles
successfully.

I've read the EW430_CompilerReference.pdf manual, but other than
the (seemingly random) __even_in_range() intrinsic, it doesn't
say much about controlling the code generated from switch/case
statements.

Can anyone shed some light on this? As a fallback, I could create
a whole mess of functions and create a table of function pointers,
but that adds the call/ret overhead and more stuff on the stack.


Thanks for any suggestions...


Frank McKenney
--
    (A)bort, (R)etry, (G)o fishing?
--

  • Using your test code, I used the a later IAR Workbench Kickstart version from www.iar.com and it did not report the compiler errors you mention.

    If it is not a huge task for you, I might suggest that get the latest from IAR's website to enable using more recent compiler versions, etc.  The reported C/C++ compiler for the MSP430 that I have is:

    IAR C/C++ Compiler for MSP430
    V4.11E/W32 (4.11.5.9)

     

    This doesn't really answer your question I'm afraid.

**Attention** This is a public forum