Hi,
I need to control an LCD display using MSP430F3xx,instead of using 32K crystal, is it possible to use a HF crystal like 8MHz for
Basic Timer1 clock?.the LCD display frequency range is (0 to 300 Hz).
Thnakyou...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I need to control an LCD display using MSP430F3xx,instead of using 32K crystal, is it possible to use a HF crystal like 8MHz for
Basic Timer1 clock?.the LCD display frequency range is (0 to 300 Hz).
Thnakyou...
Chakra,
According to the datasheet, it looks like the 3xx family does NOT support 8MHz as an external crystal. It looks like it supports 32kHz crystal only.
The 4xx devices also supports LCD and higher frequency crystals, is that an option?
William
William,
Thankyou.
I am very sorry, there was a mistake.I was suppose to type MSP430F43xx..
Regards.
Yes, it is possible to source BT1 off an 8MHz HF crystal.
You could select SMCLK as BT1 source in BTCTL (BTSSEL=1 BTDIV=0) and select HFXT2 as the clock source for SMCLK in FLL_CTL1 (SELS = 1). Use a HFXT2 code example to help set up the HF crystal correctly. http://focus.ti.com/mcu/docs/mcuflashtools.tsp?sectionId=95&tabId=1538&familyId=342
**Attention** This is a public forum