Other Parts Discussed in Thread: MSP430F2252
We are finding what appears to be an oscillator capacitance issue with the MSP430F2252. We used 6pF load crystals that were tested by the manufacturer to be very close to 32.768KHz. with the proper load. After trying a few of these crystals, the processor is adding about 6pF capacitance to each crystal lead in addition to the actual internal capacitance value selected. In other words, to provide the proper 6pF load to the crystal for 32.768KHz operation, the processor oscillator capacitance selection of 1pF internal + 4pF internal phantom + 1 pF external capacitance is required.
We believe it’s not a PCB issue. We tried multiple boards with different layouts including modified board layouts and finally, just the crystal across the processor pins and it all points to the processor. For our case, a 2.2pF cap on each crystal leg, with the processor set for 1pF load capacitance, produces exactly 32.768 KHz. It should require 8pF on each leg, not 2.2pF!
As long as this characteristic is repeatable and doesn’t vary lot to lot, we can live with it. I’d just like to know what’s going on with these parts. Has anyone brought this up before?
We are using test code specifically written to change the internal oscillator cap value to 1pF or 6pF and outputting the buffered clock frequency for measurement.
We've experimented with setting 1pF and 6pF internal and with and without external caps and it's consistently adding more capacitance than specified.
Thanks...any help would be appreciated.
Bob B.