Other Parts Discussed in Thread: MSP430F2410
Hi,
I want to use pt100 RTD temperature sensor with MSPF4302410. The sensor will be connected to ADC12. The application is battery driven so the power budget is very short. The board size is also short its 24 mm X 34 mm.
I have seen following possible solution for PT100.
RTD: with 4-20mA output: XTR approach: Using XTR105
RTD: AFE approach: Using LMP90100
http://www.ti.com/ww/en/industrial/sensors/rtd/design.html
I want to know which one is most cost ,area and power effective.
Can you please send some Reference schematic for .
Regards
Irfan