Other Parts Discussed in Thread: MSP430F2274
Hi All,
Just a few questions about the ADC10 on the MSP430F2274. Recently, I have been using modules that have the ADC12 on it. As a result, I have gotten use to the flexibility and power of the ADC12. Recently, I had to use the MSP430F2274 again in a design, and unfortunately, I designed my PCB with the flexibility of the ADC12 in mind. More specifically, I did not realize that the "Repeat-Sequence-of-Channels Mode" on the ADC10 decrements from INCHx to INCH0 without the ability to select the order and number of channels sampled in the sequence like on the ADC12. My current application is battery powered and needs to be as low-power as possible. I need to sample 3 analog signals every 15 seconds or so, but unfortunately, as Murphy's Law would have it, I placed one of the analog signals on A15, and another one on A0. I don't want to have to leave the ADC on while it performs 13 channels that I don't need, and I would like to minimize CPU intervention. Any suggestions on a work-around to keep the current consumption to a minimum? Also, what happens when the ADC samples a channel that has not had the analog input enabled (i.e. several of the ports between A15 and A0 are being used for digital functions. How will the ADC treat them?)
Finally, I have always added an anti-aliasing filter on the input of each ADC channel to help improve signal integrity. The filter is usually a basic low pass with a 10K series resistor and a .1uF cap to ground. After reading the user's manual more closely, it looks like the analog inputs are shorted to ground when not being sampled. If that is the case, that would mean that the cap on my low pass filter would greatly increase the required sample time of the ADC since the cap has to recharge right? Should I take it off and let the natural low pass filter of the ADC do the filtering for me? Does anyone have any advice here?
Thanks for all your help. Sorry this post was so long.