Hi everyone:
I have two EM430F5137RF900 evaluation boards. I wanted to try wake on radio examples, under IAR. As I read on (CC430 Wake-On-Radio Functionality(SLAA459)). I just opened the ( WOR_on_CC430.eww) and tried to download and debug the code on boards via MSP-FET430UIF.
Problem is when I want to to verify all three RF modes, I use TX mode for one board(the red LED starts blinking) and for the other board I use WOR mode. As manual states :
both LEDs in WOR mode will toggle after each RF packet reception
but on the board with WOR mode LEDS are not blinking.
I do not know what the problem is, I thought maybe WOR is not supported on CC430f5137, since when run the same test with two EM430F6137RF900 evaluation boards, everything is OK.
Thanks.