i am reviewing code to used on an MSP430F212RGE device and noticed the following port initialization:
mov.b BIT3, $P2DIR
mov.b (BIT7+BIT6+BIT3), &P2SEL
...
mov.b BIT3, &CAPD
1. Is there any problem having P2DIR.bit3 = 0, P2SEL.bit3 = 1, and CAPD = 0 as the port settings for a short time, prior to setting CAPD = 1?
I do not see this combination of settings defined in the data sheet.
Thanks,
Steve