U0CTL |= SWRST;
ME1 |= USPIE0;
U0TCTL = CKPH+SSEL1+SSEL0+STC;
U0CTL = CHAR+SYNC+MM;
U0BR0 = 0x02;
U0BR1 = 0x0; // 0
U0MCTL = 0x00; // no modulation
U0CTL &= ~SWRST;
I can't transmit data without SPI. May be i doing something wrong...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
U0CTL |= SWRST;
ME1 |= USPIE0;
U0TCTL = CKPH+SSEL1+SSEL0+STC;
U0CTL = CHAR+SYNC+MM;
U0BR0 = 0x02;
U0BR1 = 0x0; // 0
U0MCTL = 0x00; // no modulation
U0CTL &= ~SWRST;
I can't transmit data without SPI. May be i doing something wrong...
Instead of this...
Aleksey Cherepanov said:U0CTL = CHAR+SYNC+MM;
Try this...
U0CTL = CHAR+SYNC+MM+SWRST;
Also be sure you have assigned the SIMO, SOMI, SCLK, etc pins to the USCI using the PxSEL register(s).
To transmit, write to U0TXBUF.
Jeff
The code does not switch the MSP pins to USART function.
You'll need something like PxSEL |= 0xyy, so the pins go from GPIO mode to USART mode. See description of the digital I/O ports in the users guide and the por tpin schematics in the device datasheet.
Also, SPI is give-and.take. To receive a byte, you'll have to send a byte. If you're not sending, the USART won't generate a clock signal and you're not receiving.
At this point I do not have the device receiving the signal SPI, connected only an oscilloscope.
This full code:
#include "msp430.h"
void main( void )
{
WDTCTL = WDTPW + WDTHOLD;
while(FLL_CTL0 & 3 );
U0CTL |= SWRST;
P1SEL |= BIT6 + BIT7;
P2SEL |= BIT1;
// U0CTL &= ~SPB;
ME1 |= USPIE0;// USPIE1;
U0TCTL = CKPH+SSEL1+SSEL0+STC;
U0CTL = CHAR+SYNC+MM+SWRST;
U0BR0 = 0x02;
U0BR1 = 0x0;
U0MCTL = 0x00;
U0CTL &= ~SWRST;
for (;;) {
while (!(IFG1 & UTXIFG0));
U0TXBUF = 0x35;
}
}
Without knowing your MSP model, I cannot tell whether your init is correct. I can only guess from FLL_CTL0 that it is a 4x family device.Aleksey Cherepanov said:P1SEL |= BIT6 + BIT7;
void init_SPI() //Config USART for SPI on MSP430AFE253
{
/* 1. Software Reset Enable */
U0CTL = SWRST;
/* 2. Initialize USART registers */
// 8bit data, SPI mode, USART is Master
U0CTL |= CHAR + SYNC + MM;
// Polarity CPOL=0, Phase CPHA = 1
// BRCLK source is SMCLK, 4pin mode (STE enabled)
U0TCTL = CKPH + SSEL1;
// USART Baud Rate Control Register
U0BR0 = 0x02; // Config. Baud Rate as UCLK/2
U0BR1 = 0;
U0MCTL = 0;
/* 3. Enable USART Module*/
// USART0 SPI Module Enable
ME1 |= USPIE0;
/* 4. Clear SWRST */
// Initialize USART state machine, SPI enable
U0CTL &= ~SWRST;
/* 5. Interrupts */
IE1 |= UTXIE0 + URXIE0; // TX and RX interrupt enable
/* Pin Function selection */
//P1.5 as SPI_MOSI
//P1.6 as SPI_MISO
//P1.7 as SPI_CLK
P1SEL |= BIT5 + BIT6 + BIT7;
//P2.0 as SPI_CS
P2SEL |= BIT0;
/* Pin Direction */
P1DIR |= BIT5 + BIT6 + BIT7;
P2DIR |= BIT0;
}
You surely won't MISO being an output :) BIT6 is wrong here. But the USART is overriding it anyway.Pfister Frederic said:P1DIR |= BIT5 + BIT6 + BIT7;
When a FET is attached and is operated in 4-wire JTAG mode (TEST pin high) all three pins are unavailable for USART operation.
Sure about CKPH? Most SPI slaves rerequire inactive-high signal (CKPL) but not CKPH.Pfister Frederic said:U0TCTL = CKPH + SSEL1;
Then you don't set STC. This means that STE is active. STE is an input to the USART and will shut-up the USART if STE is low. It is no output and not used to 'select' the slave.
Unless you operate as slave in multi-slave or as master in multi-master configuration, you should use 3-wire mode by setting STC bit. The slave chip select must be done with normal GPIO by software anyway. Sicne there are many slaves possible on one SPI bus, teh USART doesn't know which one you want to access. Controlling the slave chip select is to be done by the application software, depending on the 'high-level protocol' the slave expects.
Thanks a lot Jens-Michael Gross,
I actually didn't understand that STE was an input to the MSP But now I see, and this explains why I didn't get any signal out of my MCU...
Yes my SPI Slave requires CKPH, and the Clock is set to SMCLK with SSEL1 (BIT5).
And I did find a working configuration , I post it for anyone who might need it :
void halSPISetup(void)
{
UCTL0 = CHAR + SYNC + MM + SWRST; // 8-bit SPI Master **SWRST**
UTCTL0 = CKPH + SSEL1 + SSEL0 + STC; // SMCLK, 3-pin mode
UBR00 = 0x02; // UCLK/2
UBR10 = 0x00; // 0
UMCTL0 = 0x00; // No modulation
ME1 |= USPIE0; // Enable USART0 SPI mode
UCTL0 &= ~SWRST; // Initialize USART state machine
}
It can be found in the library used in slaa281b, check it out...
Anyway now I need to get my slave responding back to me ..
Sure? Note that TI (MSP) polarity is reverse to the Motorola polarity.So when a device requires polarity set, you usually don't have to set CKPL and v.v.Pfister Frederic said:Yes my SPI Slave requires CKPH.
Ah, sorry, I confused SSEL1 with SSEL_1m, which is mor ecommonly used as it enumerates the different bit combinations instead of combining bits. It also allows using SSEL_0, which won't set a bit at all btui still describe that you intentionally selected this and not just forgot to pick a clock.Pfister Frederic said:Yes my SPI Slave requires CKPH, and the Clock is set to SMCLK with SSEL1 (BIT5).
Be nice to him and he will. My slave always does. Sometimes it needs a slash with a whip, but he always responds to me :)Pfister Frederic said:Anyway now I need to get my slave responding back to me ..
**Attention** This is a public forum