Other Parts Discussed in Thread: MSP430G2231
Hi,
Is it safe to change the Internal load capacitance(XCAP) after the External crystal(XT1)
starts oscillating?
We have an application with MSP430G2231 using an external 32KHz Crystal.
The application has the requirement to be power cycled frequently.
and the MCU needs to be wake up & start the timer(clocked through ACLK) quickly(within 150msec).
But as you know that depending on 32KHz Crystal it takes few 10s to 100msec to start-up.
As a solution we found that when we use internal XCAP at default(1pF), the crystals start-up time
will be reduced to some extent.
But in the long run, 1pF XCAP is less to avoid the external noise.
So we are thinking to start-up the crystal after power up with default XCAP(1pF)
and then after getting proper 32Khz oscillation, change the XCAP settings to a higher value like 6pF.
We would like to know is it a good idea to change the XCAP values while the crystal is oscillating?
and if the new XCAP value gets added to the actual load capacitance of the crystal.
Regards.
Paddu