Other Parts Discussed in Thread: MAX232, MSP430FG4618, MAX3232
Hello!!!
I am doing a project using MSP430FG4618 IC and Interfaced MAX232 IC with it but it does not work following are my query
1. Can i Interface the MAX232/SP232/Max3232 for MSP430FG4618 ???
2. Any substitute IC which can be used to interface with MSP430 FG4618??
3. Is any possibility that Reset circuit of MSP430FG4618 is creating problem because some time data transmission occurs when i press reset
Please reply
Thanks in advance