Let's play guess...
How many days will we still see the banner in this page? :-)
Andrea
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Let's play guess...
How many days will we still see the banner in this page? :-)
Andrea
Until the future is now. :)
But right as I was typing this (or rather, somewhen since I opend the last bunch of tabs in teh browser for reading/answering) it has changed.
Seems like tomorrow has turned into today just a few minutes ago.
Looks like the ad came from Bangkog. (If I interpreted the table right, there should be around midnight now, but I might be a few hours off due to summer time)
I think 50% discount for BoosterPack is a much better banner.
I have just bought one. :>
Hey! I'm not crazy! You are all witness that it stayed there at least three days!!! :-)
Andrea
Yes, I've seen it too. But depending on where you put the dateline, it might have been only two days. :)Andrea Bioli said:Hey! I'm not crazy! You are all witness that it stayed there at least three days!!! :-)
But maybe your post was reminding someone that he forgot to press the upload button for the change :)
It's a nice thingy. And with 50% discount, it fits better to the LaunchPad which gives way more bang for the buck at the original prices.Mikolaj Filar said:I think 50% discount for BoosterPack is a much better banner.
I know it's a little bit OT, but I would like to hear from some expert (Jens-Michael? :-) ) what are his considerations about the new Piccolo Launchpad: from the hobbyist point of view, but even for the professional...
Is it possible? :-)
Andrea
Jens-Michael Gross said:However, I prefer to use the lifetime 100% discount code I won last year. (not that I used it much since).
I would prefer to use it too :)
Andrea Bioli said:I know it's a little bit OT, but I would like to hear from some expert (Jens-Michael? :-) ) what are his considerations about the new Piccolo Launchpad: from the hobbyist point of view, but even for the professional...Is it possible? :-)
I am not an expert but I also have thought about Piccolos. On the website there is an info the starting price for F2802x is $1.85 (1ku), but distributor's prices start from ~$3 (1ku). It means a price of single MCU is above $6 or $7. There isn' t a lot of models and quantity of peripherals doesn't shock. One advantage I have noted: not limited CCS for free.
I prefer to use ARM or DSP if I need to process signal data: more I/O, peripherals and better performance with the price of Piccolo.
Maybe power consumption is lower for Piccolo? I didn't check that.
Mikolaj Filar said:Maybe power consumption is lower for Piccolo? I didn't check that.
The F2802x requires more than 10mA's during "IDLE" and +3mA's during "STANDBY", which is a bit higher than similarly spec'd Cortex-M3, and certainly nowhere near the MSP430 :)
However, from what little I've gathered by skimming through the manuals and datasheets, the architecture appears to have single-cycle access for SRAM and certain peripherals. Not in the sense of "single" cycle load-store on the ARM, but more like the register-memory model of the MSP430, with a lot less orthogonality of course.
Also I'm a bit intrigued by this "Control Law Accelerator" thing available on some higher Piccolos, which is an independently programmable floating-point co-processor with its own code and data bus, as well as direct access to some peripherals. Interesting way to implement Asymmetrical Multiprocessing, but it does create quite a bit of complexity during development; I suppose it would be most useful in a very domain-specific setting.
Tony
Yes, maybe the most appropriate words are just your last: 'domain-specific'.
Or when the processing power needs make the difference...
Other than that, maybe it's better to stick to the MSP430... I'm falling in love with this chip! :-)
Andrea
**Attention** This is a public forum