This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB device not recognized.. MSP430

Hi,

  I am using F5529 on my own hardware. with XT2 of 12MHz . I am able to download firmware using USB (hardware method). I download the HID demo program

using USB downloader but now it says USB device not recognized. If I start the HID demo program I get an error as

"No Serial interface found for VID/PID combination (VID = 2047  PID= 301)

Please connect a board with USB on this workstation"

         If i follow the same procedure on development board, it works.

 

Thanks

**Attention** This is a public forum