Other Parts Discussed in Thread: MSP430F2619
I've been trying to program an MSP430 2619 but every time I debug, i get the error message Error connecting to the target:
Unknown device. I am using the MSP-FET430UIF and have tried downgrading back to V2 and using CCS v4 as well as upgrading to v3 and using CCS v5 all with no luck. I'm taking over a project, and the board worked about 2 months ago so it isn't the design. I have also tried two different chips, still with no luck. Any help would be greatly appreciated!
I forgot to add; it shows up as COM10 in the Device Manager, I have tried switching the ports with no avail. I have also re-installed the drivers for the FET. My board has UART/USB on it and when I connect the uC to the computer via the UART I get confirmation (via two Rx/TX LEDs). A few months ago, the last program loaded was just an ECHO program and as of a few weeks ago that was still working. Since then I did something to erase the chip because now I still get the blinking LEDs but it doesn't echo my inputs any more.