Other Parts Discussed in Thread: MSP430F1612, TXB0304, TXB0304EVM, TUSB3410
Hi, i got a project with a MSP430 that is powered with 3V. While i got no real FET i am using the LaunchPad to program my device. It is working, however not within datasheet conditions, as LaunchPad is powered by 3.6V but pins voltage should be at most 3V + 0.3V. Is there any simple and safer way to program my device with LaunchPad? I was considering changing LaunchPad LDO feedback resistors to reduce the supply voltage but i guess i will have problems due to the 12Mhz crystal. Actually looking at the Datasheet the MSP430F1612 should use a max frequency of 8Mhz. How is that possible? Is it overclocked?
Best regards,
Luis Filipe Rossi