This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiling BSL Scripter Source code.



What compiler was used for the BSL scripter?I tried compiling it with VS2010 C++ and it gives some error.

I need to invert the action of the RTS and DTR because I created a minimal hardware circuit for BSL (it works fine with some inverters but I would like to remove it).

I hope there is an option to invert this two lines by a command on the script . py-msp430-tools has this option to invert this two lines as well as swap them. Ill be using this in production, and I dont want to install python on the machines as it will be easier to distribute the bsl_scripter.exe.

Thanks

**Attention** This is a public forum