Hello everybody,
I have installed DescriptorTool-3_20_00-Linux-x86-Install under Linux 64bit (Ubuntu). The installation was without any problem. But when I tried to start the tool it failed with the following message in the console:
/usr/lib/gio/modules/libgioremote-volume-monitor.so: wrong ELF class: ELFCLASS64
Failed to load module: /usr/lib/gio/modules/libgioremote-volume-monitor.so
/usr/lib/gio/modules/libgvfsdbus.so: wrong ELF class: ELFCLASS64
Failed to load module: /usr/lib/gio/modules/libgvfsdbus.so
/usr/lib/gio/modules/libgiogconf.so: wrong ELF class: ELFCLASS64
Failed to load module: /usr/lib/gio/modules/libgiogconf.so
and a message window with the following text:
JVM terminated. Exit code=13
/usr/bin/java
-jar /usr/local/MSP430_Descriptor_Tool_3_20_00/plugins/org.eclipse.equinox.launcher_1.1.0.v20100507.jar
-os linux
-ws gtk
-arch x86
-showsplash
-launcher /usr/local/MSP430_Descriptor_Tool_3_20_00/MSP430_USB_Descriptor_Tool
-name MSP430_USB_Descriptor_Tool
--launcher.library /usr/local/MSP430_Descriptor_Tool_3_20_00/plugins/org.eclipse.equinox.launcher.gtk.linux.x86_1.1.1.R36x_v20100810/eclipse_1309.so
-startup /usr/local/MSP430_Descriptor_Tool_3_20_00/plugins/org.eclipse.equinox.launcher_1.1.0.v20100507.jar
-exitdata 25801e
-vm /usr/bin/java
-vmargs
-jar /usr/local/MSP430_Descriptor_Tool_3_20_00/plugins/org.eclipse.equinox.launcher_1.1.0.v20100507.jar
It looks to me as there were a problem with some librarys and their 32bit version. ia32 is installed.
What do I need to do to make it work?
Thank you a lot for your help.
Greetings Reto