Other Parts Discussed in Thread: MSP430FR5728, MSP430G2452
Hello,
I only need one channel ECG, and I am going to use 1291 in my application, to reduce the cost and size of my application, I want to use msp430FR5728 or 38. the major function of this MCU is communicate with 1291 and a handheld device through UART, and related DSP( no USB and display). I don't know how to evaluate the calculation requirement of notch filter and band pass filter. the demo board is 128K flash, 8+2K ram. I hope I can use 5728/5738, is it possible? how to evaluate this calculation load?
another option of my application is to use a low end MSP like MSP430G2452, to convert SPI to UART. then my question becomes how much calculation power does host device need. I know it is hard to answer the question. let's assume that the host is a Samsung smart phone or Iphone, is it possible for them to handle DSP calculations as in EVM? is it only use a fraction of smart phone power, or it barely can handle it?
thank you,
David