http://www.ti.com/lit/ds/symlink/msp430g2553.pdf (SLAS735G-APRIL 2011-REVISED AUGUST 2012)
page 56:
What is the usefulness of such a link in green? It exists on all ports, the P3.0 was used because it is the simplest.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
http://www.ti.com/lit/ds/symlink/msp430g2553.pdf (SLAS735G-APRIL 2011-REVISED AUGUST 2012)
page 56:
What is the usefulness of such a link in green? It exists on all ports, the P3.0 was used because it is the simplest.
It looks like when PxSEL2 = 1 and PxSEL = 0 then it has the pull up/down resistor enabled and if the input is 1 then it pulls it down and when input is 0 then it pulls it up.
In http://www.ti.com/lit/ug/slau144i/slau144i.pdf on page 337 there's a table that says:
My impression is that it is a feedback which is part of the bus keeper logic. That means, if the input goes to a floating or high impedance status, that logic keeps the input at its last driven value.
I too reported this strange 'shortcut' soem tiem ago as a possible bug in teh documentation.
I too suspected it to be a misdrawn bus-keeper logic, but on other port pins there is a bus keeper (here is none because of the pinosc feature. i think) and still this strange connection.
So I don't know what its meaning is. From a plain schematics view, it must be an error, as it maks the output of the module fighting the output of the input.
**Attention** This is a public forum