Hello,
I just broke my DRV8825 prototype board (designed by me). It was a simple project: DRV8825 with goldpins for control, power supply etc.
I wanted to control it from launchpad but I didn't connect Launchpad GND with DRV8825 GND. I measured DC voltage between these two GNDs and it was ~0,5V difference. I ran it and I'm sure in this way I broke the driver. When I measure AC voltage between GNDs it was 10V. :/
My problem is:
In DRV88xxEVM I see that DRV GND and USB GND are probably* connected. Is it safe? It can cause that all current from motor will flow to USB GND and I think there are any limits for flowing current?
*probably because in the schematic some GND symbols are signed "GND" and these ones from DRV not.
Best regards,
Mikolaj