Hi all,
I've been using the BM Innovation tool for burning rFbSL and program code in CC430f6137. Earlier the BM tool was erasing the main memory as well as the information memory. But now after some change in code, without touching the debugging/burner option of IAR. I used the generated .txt file as earlier. The information is not going away. May be the code flow difference.
Is there any option in BM tool (its scripts) so that I can force it remove the information memory of the CC430f6137?