Hi there,
Is there an application note available on how to interface a character LCD to MSP4304794 or MSP430F6x
Thanks in advance
Claus
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
Is there an application note available on how to interface a character LCD to MSP4304794 or MSP430F6x
Thanks in advance
Claus
Hi Claus.
I think you are looking for a solution which can drive 4 x 24 LED characters meaning 4 x 24 x 7 segments which is above the capability for MSP430.
BR
Anders Lange
In this forum there are several threads about interfacing alphanumeric LCD with an included standard controller.Claus Ludvigsen said:Is there an application note available on how to interface a character LCD to MSP4304794 or MSP430F6x
The posted code in these threads is for 1x16 or 2x16, but it should not be difficult to change it to support more lines of more chars, as long as the controller is the same or compatible.
The 4x series MSPs are for directly interfacing controllerless glass LCD. Here the limit is 192 segments (48x4 multiplexed). Which isn't sufficient for character display at all (a single full graphical character takes 48 to 64 segments depending on pixel resolution). It is rathe rmeant for pre-shaped icons and 7-segment numerical displays.
**Attention** This is a public forum