If I need to use both the RTC and UART, do I need 2 crystals? Can I use just a 32khz crystal for the RTC and do a frequency multiplication for the UART with the fr5739 part?
Thanks,
Carl
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If I need to use both the RTC and UART, do I need 2 crystals? Can I use just a 32khz crystal for the RTC and do a frequency multiplication for the UART with the fr5739 part?
Thanks,
Carl
Hi,
you can use even the internal calibrated DCO as the clock source for the UART.
Please refer to the MSP430FR57xx Family User's Guide - http://www.ti.com/lit/ug/slau272a/slau272a.pdf - Table 18-5. Recommended Settings for Typical Crystals and Baudrates at page 436. There you can find that even using the internal DCO clock, you can achieve relatively very low error percentage on UART communication.
I hope this helps.
I see Table 18-5. Recommended Settings for Typical Crystals and Baudrates. Is the BRCLK frequency referring to te crystal frequency or the DCO frequency?
Hi,
i think you need the 32kHz for the RTC module, but not for the UART. Please refer to the MSP430FR57xx Family User's Guide, SLAU272 - chapter 3 (especially look at the block diagram shown in Figure 3-1).
Table title says Table 18-5. Recommended Settings for Typical Crystals and Baudrates
So is the BRCLK in the table referring to the crystal frequency or the DCO frequency? I was checking the error rate but wasn't sure if it was the error rate for different crystals or different DCO frequencies.
Hi,
the BRCLK in Table 18-5 is basically input clock frequency of the eUSCI module. Please refer to the Figure 18-1. "eUSCI_Ax Block Diagram – UART Mode (UCSYNC = 0)." in the same document.
**Attention** This is a public forum