This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

P2.6 will not work - altering flashing LED file for P2.6 output

Other Parts Discussed in Thread: MSP430F2002

I have altered the Flashing the LED example code to flash a LED connected to the port P2.6. I can toggle all the 1.x ports, but not the 2.x ports....

I am using the MSP430F2002, have specified this in the Projects>Options...> Target. 

An ideas as to what I am doing wrong???

Here's the file:

#include "msp430.h"
;-------------------------------------------------------------------------------
ORG 0FC00h ; Progam Start (1K Flash device)
;-------------------------------------------------------------------------------
RESET      mov.w      #0280h,SP                                             ; Set stackpointer (128B RAM device)
StopWDT  mov.w      #WDTPW+WDTHOLD,&WDTCTL     ; Stop watchdog timer
SetupP1    bis.b        #000h,&P1DIR                                       ; Set P1.0 to input direction
                    bis.b        #00h,&P2SEL                                        ; Set P2.x to output
SetupP2    bis.b        #0F0h,&P2DIR                                       ; Set P2.6,2.7 to output direction

Mainloop   xor.b         #0FFh,&P2OUT                                     ; Toggle P2.6
Wait           mov.w       #050000,R15                                         ; Delay to R15
L1              dec.w        R15                                                           ; Decrement R15
                   jnz              L1                                                             ; Delay over?
                   jmp           Mainloop                                                  ; Again
;
;-------------------------------------------------------------------------------
; Interrupt Vectors
;-------------------------------------------------------------------------------
ORG 0FFFEh ; MSP430 RESET Vector
DW RESET ;
END

**Attention** This is a public forum