Hi:
I am building a stand along board using MSP430G2453 while using CCS5 and the Launchpad to develop the software. When I build and debug the software within CCS, everything works fine. After done and tested the software, I disconnect the board from the Launchpad and in turn powering the board using a 3.7V battery. Once the board is in the stand alone mode, the software on the board is no longer working.
I am wondering if I am missing some steps to make the board work in a stand alone mode. Please help and this is somewhat urgent.
Thanks very much in advance.
--Neo